QSB HW reset button

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSB HW reset button

2,767件の閲覧回数
AnthonyTong
Contributor I

I already own a QSB with Dialog DA9053 PMIC and today I received my new QSB with MC34708 PMIC. I found that I couldn't reset the board by pressing the reset button on the board. Did anyone have this issue before and what is the solution? Did I miss a patch to u-boot or kernel so the reset signal doesn't route to the chip correctly?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,485件の閲覧回数
MiroslavIMX53QS
Contributor I

I have a same problem with my QSB, and this is not deterministic behavior, sometimes it just works with one click, but the other times I have to hold a button longer.

0 件の賞賛
返信

2,485件の閲覧回数
AnthonyTong
Contributor I

I've just found out I need to hold a button for about 10 sec to reset. Thank you for your replies.

0 件の賞賛
返信

2,485件の閲覧回数
TheAdmiral
NXP Employee
NXP Employee

The reset button should be working on the MX53 Quick Start board. Are you using the same boot code for both boards? You need to be using the START-R code that came with the new board. The two codes are not compatible.

0 件の賞賛
返信

2,485件の閲覧回数
MiroslavIMX53QS
Contributor I

Did you try to hold a button pressed for some time (5 - 10 sec)?

0 件の賞賛
返信