QCA6174 for 5.4 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QCA6174 for 5.4 kernel

5,254 次查看
manizillion
Contributor IV

Will QCA6174 drivers work for imx8mqevk on 5.4 kernel linux-fslc-imx ? for bluetooth and wifi

 

 

标签 (1)
0 项奖励
回复
5 回复数

5,242 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Manizillion,

 

The Qualcomm driver firmware-qca-3.0.2.bin i.MX QCA Bluetooth Wi-Fi firmware is included in the L5.4.24_2.1.0 BSP. This is the latest with that firmware in it.

 

Regards

 

0 项奖励
回复

5,231 次查看
manizillion
Contributor IV

 

破坏者
 

Sir , Thanks

 

I have added the drivers on the build and see the following files in the path, Is the modules OK or anything is missing.

What is the command to enable the qca bluetooth adapter on the console ?

./lib/firmware/qca6174
./lib/firmware/wlan/qca6174
./lib/modules/5.4.51+gcfe6dd72/extra/qca6174.ko

0 项奖励
回复

5,201 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

In 5.4.47 is not enable by default QCA supports Wi-Fi through firmware provided with firmware-imx software and BCM supports firmware provided with imxfirmware at imx-firmware github

https://github.com/nxp/imx-firmware

 

 

0 项奖励
回复

5,190 次查看
manizillion
Contributor IV

I am using Linux version 5.4.51 , how to enable QCA 6174 in this kernel? Can you please share steps for this 

Is it possible ?

0 项奖励
回复

4,991 次查看
alj79
Contributor II

The same question, any answer?

How to resolve it?

0 项奖励
回复