QCA6174 for 5.4 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCA6174 for 5.4 kernel

5,238件の閲覧回数
manizillion
Contributor IV

Will QCA6174 drivers work for imx8mqevk on 5.4 kernel linux-fslc-imx ? for bluetooth and wifi

 

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

5,226件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Manizillion,

 

The Qualcomm driver firmware-qca-3.0.2.bin i.MX QCA Bluetooth Wi-Fi firmware is included in the L5.4.24_2.1.0 BSP. This is the latest with that firmware in it.

 

Regards

 

0 件の賞賛
返信

5,215件の閲覧回数
manizillion
Contributor IV

 

スポイラ
 

Sir , Thanks

 

I have added the drivers on the build and see the following files in the path, Is the modules OK or anything is missing.

What is the command to enable the qca bluetooth adapter on the console ?

./lib/firmware/qca6174
./lib/firmware/wlan/qca6174
./lib/modules/5.4.51+gcfe6dd72/extra/qca6174.ko

0 件の賞賛
返信

5,185件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

In 5.4.47 is not enable by default QCA supports Wi-Fi through firmware provided with firmware-imx software and BCM supports firmware provided with imxfirmware at imx-firmware github

https://github.com/nxp/imx-firmware

 

 

0 件の賞賛
返信

5,174件の閲覧回数
manizillion
Contributor IV

I am using Linux version 5.4.51 , how to enable QCA 6174 in this kernel? Can you please share steps for this 

Is it possible ?

0 件の賞賛
返信

4,975件の閲覧回数
alj79
Contributor II

The same question, any answer?

How to resolve it?

0 件の賞賛
返信