Hi,
On my evk am trying to enable PWM for controlling LEDs,
After going through post IMX8MM-EVK-pwm-output
I have made following changes,
pinctrl_pwm1: pwm1grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO01_PWM1_OUT 0x16
>;
};
pinctrl_pwm2: pwm2grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO13_PWM2_OUT 0x16
>;
};
pinctrl_pwm3: pwm3grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO14_PWM3_OUT 0x16
>;
};
pinctrl_pwm4: pwm4grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO15_PWM4_OUT 0x16
>;
};
.
.
.
.
&pwm1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm1>;
status = "okay";
};
&pwm2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm2>;
status = "okay";
};
&pwm3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm3>;
status = "okay";
};
&pwm4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm4>;
status = "okay";
};
Kernel Configs enabled:
Symbol: LEDS_PWM [=y]
│ Type : tristate
│ Prompt: PWM driven LED Support
│ Location:
│ -> Device Drivers
│ (9) -> LED Support (NEW_LEDS [=y])
│ Defined at drivers/leds/Kconfig:513
│ Depends on: NEW_LEDS [=y] && LEDS_CLASS [=y] && PWM [=y]
For starters am planning to Control PWM signal from sysfs..
What is the procedure to up the PWM imx8mm-evk? Is there any step-by-step guide available?
Why there is no proper documentation available like application note from NXP??
Solved! Go to Solution.
Hello autoamp,
I am Nitin B S who is also trying to enable PWM in imx8m plus evk through sysfs. I am activating my pwmchip and pwmchannel and running the code. The code is being executing as expected but when i connect the LED to board the results are not being reflected in my LED it is not even turning on.
I am connecting my LED as shown in the config below to pin number 32(PWM4).
Can you please help me regarding the issue.
Thanks and Regards
Nitin B S
Thanks for the response... Issue resolved alredy