Python code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,886件の閲覧回数
1990rahulreddy
Contributor IV

How can I run Helloword.py, in YOCTO. I have qt image installed in SABRE-SDP.

Is there new ubuntu launch for i.MX6. I know older ubuntu(11. #).

ラベル(3)
0 件の賞賛
返信
1 解決策
4,641件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

1990rahulreddy​, you should be able to access the document now.

Installing Ubuntu Rootfs on NXP i.MX6 boards

Regards,

元の投稿で解決策を見る

5 返答(返信)
4,206件の閲覧回数
卢金磊
Contributor I

@1990rahulreddy 你好,该问题是否解决,有没有具体的方案,我这边python一直不能支持

0 件の賞賛
返信
4,641件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rahul Reddy ,

Yocto allows you to build a Linux root file system for your board. You may run post-scripts while building your image in Yocto as part of the image recipe, is this what you’re looking after? It would seem that you rather want to run a script on the Qt image, which would be a different procedure and you would need to make sure that you have Python installed on the Qt image.

There is not an official Ubuntu BSP for the i.MX6, however, you may follow the instructions on the following document to load an Ubuntu RootFS on the i.MX6.

Installing Ubuntu Rootfs on NXP i.MX6 boards

Regards,

0 件の賞賛
返信
4,641件の閲覧回数
1990rahulreddy
Contributor IV

Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here

0 件の賞賛
返信
4,641件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rahul Reddy,

I'm very sorry. I've escalated this so the document gets the right access settings so you may access it. It should be ready in a couple of hours.

Regards,

0 件の賞賛
返信
4,642件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

1990rahulreddy​, you should be able to access the document now.

Installing Ubuntu Rootfs on NXP i.MX6 boards

Regards,