Proper way to modify imx/aosp kernerl with git?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Proper way to modify imx/aosp kernerl with git?

1,614 次查看
lshi
Contributor I

I want to make a customized kernel for Android p9.0.0_2.3.0. I see the kernel source is located at 

vendor/nxp-opensource/kernel_imx

git remote shows 

https://source.codeaurora.org/external/imx/linux-imx 

git status shows:

Not currently on any branch.

git branch shows:

* (no branch)

inside .repo/manifest/imx-p9.0.0_2.3.0.xml

<project path="vendor/nxp-opensource/kernel_imx" name="linux-imx" remote="imx-linux-sdk" revision="refs/tags/p9.0.0_2.3.0" />

I am thinking to create a branch and push my github, but how to do it properly so the repo can sync/update them together?

标签 (1)
0 项奖励
回复
2 回复数

1,561 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Lei,

The android 9 works with that version of the kernel and there is no modification about nxp, if you need to modify the kernel you should work with android provided by google.

regards

0 项奖励
回复

1,561 次查看
lshi
Contributor I

Hi there,

Well, I want to replace the kernel logo (the penguin) with my own. I searched the forum and it seems to me that I have to rebuild the kernel since the old patch doesn't work. Is "vendor/nxp-opensource/kernel_imx" the one I need to work with? Or any other ways?

thanks,

Lei

0 项奖励
回复