Programming eMMC via JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming eMMC via JTAG

4,124件の閲覧回数
rsk_11
Contributor III

I am using iMX8QXP.

My query is can we flash the binaries( SECO,SCU,UBOOT,M4 APP,AP LINUX etc)
on the target board eMMC using JTAG?

We donot have SDCard or USB connection, hence is programming of eMMC via JTAG is possible?

Kindly provide any links or documents for help if any.


Thanks!

 

0 件の賞賛
返信
3 返答(返信)

4,102件の閲覧回数
rsk_11
Contributor III

Thankyou for the reply.

The readme has steps for loading ATF and Uboot. Please find following queries for the same:

1. How to load a SCU FW scm_tcm.bin ?

2. Does the given .cmm script load the ATF and Uboot in given example to eMMC on MEK for iMX8QXP?

3. On our custom board we are using a different eMMC than the one used on MEK, How to generate .cmm for a different eMMC?

 

Regards.

 
0 件の賞賛
返信

4,072件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you should already get all of information from internal team, I will close this case then

0 件の賞賛
返信

4,104件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can use trace32 to download scfw to the board, then use uboot to download images, see the attached readme

 

0 件の賞賛
返信