Programming ZMK on i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Programming ZMK on i.MX6

1,651 次查看
hughboddington
Contributor I

I'm trying to program the ZMK on the i.MX6 but just can't get it to work.  I must be missing something simple.

- The system is secure booting in "closed" mode.  

- hab_status reports no errors in u-boot

- SSM_ST of SNVS_HPSR is 1101 - "trusted"

- ZMK_WSL and ZMK_RSL of SNVS_HPLS are not set (ZMK is writeable and readable)

- ZMK_RHL and ZMK_WHL of SNVS_LPLR are not set

- ZMK_ZERO is true

- ZMK_HWP of SNVS_LPMKCR is false (software programming mode)

- The processor is executing in Supervisor mode 

- I write a test pattern to the ZMK registers (0x20CC06C - 0x20CC08C) using 32-bit writes

- When I read back, I get 0x00, and ZMK_ZERO is still true

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,435 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled

as a Service Request.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复