Programming WinCE in eMMC, i.MX53SMD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming WinCE in eMMC, i.MX53SMD

1,481件の閲覧回数
AbisaiNegrete
Contributor II

Using Mfg1.6.2.042 tools and selected <MX53 WinCE Update\SMD> profile I tried to reflash the MMC that has android for now.

But after MfgTool has finished without any error, I re-boot the board and it still runs u-boot, that means the mfg failed to erase/program eMMC.

0 件の賞賛
返信
1 返信

1,024件の閲覧回数
ChrisWilliamson
Contributor III

First of all, WinCE has no idea of how to erase an Android media. My suggestion  would be to edit the ucl.xml file in the Android profile so that it quits after erasing the media. Then move to the WinCE profile and make sure you select the eMMC list in the ucl.xml file. It is typically not an easy thing to do to go between Linux/Android and WinCE. It is best to use seperate media for each OS if you have that option.

Chris

0 件の賞賛
返信