Programming SGTL5000 Stereo Codec

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming SGTL5000 Stereo Codec

跳至解决方案
2,285 次查看
jamesmin
Contributor II

Hi. I am writing driver code for SGTL5000 audio codec. The voltage I am using for the codec is VDDIO=3.3v, VDDA=3.3v and VDDD=1.8v.

As the voltage level is different from other reference board, I want someone double check the register values that needs to be configured for my case. The values I am trying to use is like below.

Write CHIP_ANA_POWER 0x4260

Write CHIP_LINREG_CTRL 0x006C

Write CHIP_REF_CTRL 0x01FF

Write CHIP_LINE_OUT_CTRL 0x0322

Write CHIP_REF_CTRL 0x004F

Write CHIP_SHORT_CTRL 0x1106

Write CHIP_ANA_CTRL 0x0133

Write CHIP_ANA_POWER 0x6AFF

Write CHIP_DIG_POWER 0x0073

Write CHIP_LINE_OUT_VOL 0x0505

As I use external VDDD. Can you check whether any additional value needs to be applied?

Also I want to know whether external VDDD can be used on the latest SGTL5000 device (revision:0x11).

Thank you.

James.

标签 (1)
0 项奖励
回复
1 解答
1,965 次查看
igorpadykov
NXP Employee
NXP Employee

Hi James

please look at AN3663 SGTL5000 Initialization and Programming

http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf

external VDDD should be applied according to

http://cache.freescale.com/files/analog/doc/errata/SGTL5000ER.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,966 次查看
igorpadykov
NXP Employee
NXP Employee

Hi James

please look at AN3663 SGTL5000 Initialization and Programming

http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf

external VDDD should be applied according to

http://cache.freescale.com/files/analog/doc/errata/SGTL5000ER.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复