Hi All:
We encountered a problem when programing kernel to the NAND flash of our iMX233 CPU module. We have about 10% fail cases when flashing the kernel to the NAND (we built 22xx pcs and have over 170 pcs NAND write fail). The NAND Flash that we are using is Samsung K9F1G08U0D.
We use the kobs-ng tool to flash the NAND. We first boot the Board with SD Card and write the kernel to the NAND.The below error message is from the first time programming:
Programing Bootloader...
mtd: device 0 fails MEMERASE (0x460000 - 0x20000)
mtd: Failed to erase block @0x460000
We tried to use the following command to program after encountered this error message:
echo 1 > /sys/devices/platform/gpmi-nfc.0/ignorebad
flash_eraseall /dev/mtd0
The following messages are get from the terminal:
flash_eraseall has been replaced by `flash_erase <mtddev> 0 0`; please use it
Erasing 128 Kibyte @ 460000 -- 31 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 35 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 128 Kibyte @ de0000 -- 100 % complete
Followed by the following Message
echo 1 > /sys/devices/platform/gpmi-nfc.0/ignorebad
flash_eraseall /dev/mtd0
flash_eraseall has been replaced by `flash_erase <mtddev> 0 0`; please use it
flash_erase: Skipping bad block at 00000000
flash_erase: Skipping bad block at 00020000
flash_erase: Skipping bad block at 00040000
flash_erase: Skipping bad block at 00060000
flash_erase: Skipping bad block at 00080000
flash_erase: Skipping bad block at 000a0000
flash_erase: Skipping bad block at 000c0000
flash_erase: Skipping bad block at 000e0000
Erasing 128 Kibyte @ 440000 -- 30 % complete flash_erase: Skipping bad block at 00460000
Erasing 128 Kibyte @ de0000 -- 100 % complete
Then we entered:
echo 1 > /sys/devices/platform/gpmi-nfc.0/ignorebad
kobs-ng init /tmp/imx233_linux.sb
mtd: device 0 fails MEMERASE (0x460000 - 0x20000)
mtd: Failed to erase block @0x460000
We then power off the board. Configure it to NAND Boot, then we've got:
PowerPrep start initialize power...
Battery Voltage = 0.52Vwï¿þø
PowerPrep start initialize power...
Battery Voltage = 1.52Vßÿxð
PowerPrep start initialize power...
Battery Voltage = 0.88V
No battery or bad battery detected!!!.Disabling battery voltage measurements./r/nSep 18 201217:38:03
EMI_CTRL 0x1C084040
FRAC 0x92926192
init_ddr_mt46v32m16_133Mhz
Init Hynix HY5DU121622DT DDR SDRAM @ 133MHz
power 0x00820710
Frac 0x92926192
start change cpu freq
hbus 0x00000003
cpu 0x00010001
0x8050100b
0x80502008
Then it reboots periodically with the same message.
Does anybody have any idea? It seems the NAND write is influenced by the bad block problem. Thanks in advance.
Patrick