Profiles imx 35 for application mgftool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Profiles imx 35 for application mgftool

1,343件の閲覧回数
nico70
Contributor I

Hello,

I use application mfgtool with the imx35 but the problem is to realize the application profile for the imx 35, that does not exist in my version.

My objective is to download an image in the NAND flash of my platform.

I search an example or a profile for this imx35 for MFGTOOL

Nico

タグ(4)
0 件の賞賛
返信
1 返信

1,199件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Nicolas,

The i.MX35 does not use the MFGTool, it instead uses ATK (Advanced ToolKit), you can download it from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX353&nodeId=018rH3ZrDR633D&fpsp=1&...

Under: Hardware Development Tools --> Programmers --> IMX_ADVANCEDTOOLKIT

0 件の賞賛
返信