Processing flow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,556件の閲覧回数
takashitakahash
Contributor III

Hi community.

Discribed on IMX6DQ RM of 37.1.2.1.4 Processing of Table 37-5. Time-Shared Data Flow through the IPU.

Defined in Table 37-5, DSx and PLx, VFx, RCx, GFx is not possible to use only Flow of figure?

Also whether , Can I set another Flow?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

only flows described in Table 37-5 are time shared, "another Flow"

will not be time shared. Also from Comments to Table 37-5:

• Time-sharing

• IC can time-share tightly three flows: one VFx, one RCx and one PLx (with

independent processing parameters)

• DP can time-share one DS1 flow and a one DS2 flow (each with different

destinations and independent processing parameters)

• Direct access to display (DS4) time-shares tightly the display port with other

active DSx flows.

• Other time-sharing (between PLx flow and DS2 and DS3 flows in IRT) is frameby-

frame

• Any of the processing stages in the above flows can be skipped.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,518件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

only flows described in Table 37-5 are time shared, "another Flow"

will not be time shared. Also from Comments to Table 37-5:

• Time-sharing

• IC can time-share tightly three flows: one VFx, one RCx and one PLx (with

independent processing parameters)

• DP can time-share one DS1 flow and a one DS2 flow (each with different

destinations and independent processing parameters)

• Direct access to display (DS4) time-shares tightly the display port with other

active DSx flows.

• Other time-sharing (between PLx flow and DS2 and DS3 flows in IRT) is frameby-

frame

• Any of the processing stages in the above flows can be skipped.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信