Dear sir,
I install LTIB .As per the mx53 start linux bsp user guide.pdf in
step 2.2 upto step install one package to rootfs
(./ltib -m scdeploy -p u-boot) done successfully.
After that I go to section 7 using a linux host to set up an
microSD card. complete all the steps (screen shots are attached
here).
Then go to step 8.2 Run the image from MMC/SD. In that I connect vga
display to QSB. Connect serial port to my windows PC and configure it
to 115200-8-N-1 . press "POWER " key to power up the board but it
does not show any thing on VGA display as well as on hyperterminal.
Please check the attachment and guide me what is the problem
Thank you
swapneel