Problems setting eclipse for imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems setting eclipse for imx6ul

ソリューションへジャンプ
2,289件の閲覧回数
alexishernandez
Contributor III

Hi, i followed the steps in

Setting up the Eclipse IDE for Yocto Application Development​

but i'm stuck at the "Reconfigure Project" step, i got this output when make this156096_156096.pngScreenshot from 2016-07-20 07_55_33.png
I chmod the workspace file to have 'rwx' permissions also i got the 2.1 yocto plugin version and the toolchain that i'm using is the corresponding to the image target (at least is what i think)156097_156097.pngScreenshot from 2016-07-20 08_07_14.png

Toolchain:core-image-sato-armv7a http://downloads.yoctoproject.org/releases/yocto/yocto-2.1/toolchain/i686/

Image: bitbake core-image-sato
Machine: imx6ulevk

Really need help with this one, thanks and regards

ラベル(2)
0 件の賞賛
返信
1 解決策
1,967件の閲覧回数
alexishernandez
Contributor III

Hi weidong.sun

     Thanks for your answer, the issue seems to be a mismatch between the sdk toolchain and the sysroot file, this can be solved by building your own sdk toolchain (see Appendix A.2 from sdk manual).
Hope someone find this thread helpful.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,967件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Alexis,

   Ecllipse IDE is not our product, so it is not in the scope of support, but according to above log, I can give you some advice.

From No.1 screenshot, It seems that Makefile file should be needed for your application, so "no rule to make target" was reminded.

For more detailed about Ecllipse on how to create a Makefile, see here:

Help - Eclipse Platform

Hope above information can help you!

Best Regards,

Weidong

0 件の賞賛
返信
1,968件の閲覧回数
alexishernandez
Contributor III

Hi weidong.sun

     Thanks for your answer, the issue seems to be a mismatch between the sdk toolchain and the sysroot file, this can be solved by building your own sdk toolchain (see Appendix A.2 from sdk manual).
Hope someone find this thread helpful.

0 件の賞賛
返信