Problems on aiurdemux with dvb incoming stream

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems on aiurdemux with dvb incoming stream

2,197 次查看
jordanguillot
Contributor II

Hi community,

The setup is the following:

rootfs built with yocto daisy, and MACHINE is imx6dlsabresd.conf, linux kernel is 3.10.53.

I have to use gstreamer-0.10.

I try to use gstreamer to watch french terrestrial télévison via USB TV tuner

I use the following pipeline:

gst-launch dvbsrc adapter=0 inversion=AUTO modulation=AUTO trans-mode=AUTO bandwidth=8 frequency=754000000 code-rate-lp=AUTO code-rate-hp=AUTO guard=AUTO hierarchy=AUTO

! "video/mpegts, systemstream=(boolean)true, packetsize=(int)188" \

! aiurdemux \

! queue2  \

! vpudec \

! imxv4l2sink

But, recently in France, the terrestrial TV switched to only HD TV stream. Since this transfer, aiurdemux plugin doesn't work:

Aiur: 4.0.2

Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.24  build on Jul  4 2014 04:54:05

  mime: video/mpeg, mpegversion=(int)[1,2]; video/mpegts, systemstream=true; video/x-cdxa

  file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1

Content Info:

    Seekable  : No

    Size(byte): -1

ERROR: from element /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.

Additional debug info:

aiurdemux.c(4472): aiurdemux_push_task (): /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0:

streaming stopped, reason error

I try to find what's going on. I think the problem comes from Program Map Table which has change.

In the plugin "dvbsrc", I just select the pids needed like "pids=100:120:130" (100=PMT 120=Video 130=Audio), but i think the PMT is not updated from the filtered stream incoming. Thus, do you know a way to make aiurdemux work?

Best Regards,

Jordan

标签 (4)
0 项奖励
回复
4 回复数

1,961 次查看
jordanguillot
Contributor II

I don't try Gst 1.0 but update to 1.0 is in next tasks.

Best regards,

Jordan

0 项奖励
回复

1,961 次查看
jordanguillot
Contributor II

Hi,

The problem comes from "CreateParser2"(used by aiurdemux) which is in libfslparser. Thus, if I update the libfslparser from 4.0.2 to 4.0.8(last), there is no more problem.

Thank you.

Jordan

0 项奖励
回复

1,961 次查看
joanxie
NXP TechSupport
NXP TechSupport

ok, did you try gstreamer 1.0? in current bsp, we suggest customer to use 1.0 version, because we don't update 0.1 version anymore.

0 项奖励
回复

1,961 次查看
joanxie
NXP TechSupport
NXP TechSupport

it seems freescale plugin doesn't work for this, you can try to use other plugins,

for more detailed information, I found a link maybe is useful for you .

<https://www.raspberrypi.org/forums/viewtopic.php?t=62949&p=469793>.

0 项奖励
回复