Problems in detecting MINISASTOCSI in i.mx8mp plus evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems in detecting MINISASTOCSI in i.mx8mp plus evk board

ソリューションへジャンプ
1,902件の閲覧回数
kenizgandhi
Contributor III

Hello,  I am using i.mx8m plus evk board. I have connected minisastosci to my board in mipi-csi1. But when I list my devices, I am getting the following output: 

root@imx8mpevk:/dev# v4l2-ctl --list-devices

mxc-isi-m2m (platform:32e00000.isi:m2m_devic): /dev/video0

This is the output I am getting after I type the below command : 

root@imx8mpevk:/dev# v4l2-ctl --all -d 0

[ 114.418814] Unable to handle kernel NULL pointer dereference at virtual address 000000000000000c [ 114.427646] Mem abort info: [ 114.430467] ESR = 0x96000004 [ 114.433543] EC = 0x25: DABT (current EL), IL = 32 bits [ 114.438881] SET = 0, FnV = 0 [ 114.441954] EA = 0, S1PTW = 0 2[r i v1e1r4 .I4n4f5o0:9 ] DData abort info: [ 114.449387] ISV = 0, ISS = 0x00000004 [ 114.453237] CM = 0, WnR = 0 river nam[e 11 4 . 4 5:6 2m0x4] user pgtable: 4k pages, 48-bit VAs, pgdp=00000001062d0000 [ 114.464389] [000000000000000c] pgd=0000000000000000, p4d=0000000000000000 [ 114.471210] Internal error: Oops: 96000004 [#1] PREEMPT SMP [ 114.476783] Modules linked in: fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes crct10dif_ce imx8_media_dev(C) flexcan caam can_dev secvio error [ 114.494284] CPU: 3 PID: 566 Comm: v4l2-ctl Tainted: G C O 5.10.9-1.0.0+g32513c25d8c7 #1 5-i[s i -1m124m. 0 3C4a1r2d] Hardware name: NXP i.MX8MPlus EVK board (DT) type : mxc-isi-m2m Bus info : platform:32e00000.isi:m2m_devic Driver versi[ 114.518270] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) on : 5.10.9 Capabilities [ 114.524282] pc : mxc_isi_m2m_g_fmt_vid_cap+0x48/0xb0 [ 114.531923] lr : mxc_isi_m2m_g_fmt_vid_cap+0x18/0xb0 3 : 0x8[4 2 0141040.05 68 8 4V] sp : ffff800012cebbc0 [ 114.541843] x29: ffff800012cebbc0 x28: ffff8000112cd818 ideo Memory-to-M[e m o1r1y4 .M5u47155] x27: 00000000c0d05604 x26: ffffffffffffffed [ 114.554544] x25: ffff0000c18b2088 x24: ffff8000112cd818 ltiplanar 5 Str[e a m1i1n4g. 59855] x23: ffff0000c6452e08 x22: ffff0000c757c900 6 Extended Pix [F o 1r1m4a.t5 7244] x21: ffff0000c7766900 x20: ffff0000c7766908 5 Device Capabi[l i t1i1e4s. 7 4546] x19: ffff0000c7766900 x18: 0000000000000000 evice Caps [ :1 104x.508412847] x17: 0000000000000000 x16: 0000000000000000 04000 Video M[e m o1r1y4-.t58o9149] x15: 0000000000000000 x14: 0000000000000000 -Memory Multiplan[ 11a4r. 5 9 6539] x13: 0000000000000000 x12: 0000000000000000 Streaming Extende[d P1i1x4 F603839] x11: 0000000000000000 x10: 0000000000000000 [ 114.611401] x9 : 0000000000000000 x8 : 0000000000000000 ormat 4riority[: 211 6 1712] x7 : 0000000000000000 x6 : 0000000000000000 Message from s[y s l1o1g4d.@6 2 4013] x5 : 0000000000000000 x4 : 0000000000000000 at Thu Jan 1 0[0 : 0111:43.86 31315] x3 : 0000000000000007 x2 : ffff0000c7766900 970 ... : [ [ 1 11144..4673182617] x1 : 0000000000000009 x0 : ffff0000c18b2080 10] Inte[r n1a1l4 .e6r4r5o9r:1 ] Call trace: [ 114.650011] mxc_isi_m2m_g_fmt_vid_cap+0x48/0xb0 Oops: 96000004 [[ # 111]4 .PR6E5E627] v4l_g_fmt+0xc8/0x2f0 MPT SMP [ 114.659931] __video_do_ioctl+0x180/0x3e4 [ 114.664801] video_usercopy+0x190/0x410 [ 114.668634] video_ioctl2+0x18/0x24 [ 114.672121] v4l2_ioctl+0x44/0x64 [ 114.675435] __arm64_sys_ioctl+0xa8/0xf0 [ 114.679359] el0_svc_common.constprop.0+0x78/0x1a0 [ 114.684147] do_el0_svc+0x24/0x90 [ 114.687462] el0_svc+0x14/0x20 [ 114.690514] el0_sync_handler+0x1a4/0x1b0 [ 114.694520] el0_sync+0x174/0x180 [ 114.697835] Code: b9489405 b9000e65 b9001664 f9446404 (b9400c84) [ 114.703928] ---[ end trace 9b53847cf1f19462 ]--- Message from syslogd@ at Thu Jan 1 00:01:38 1970 ... : [ 114.697835] Code: b9489405 b9000e65 b9001664 f9446404 (b9400c84) Segmentation fault

P.S. :I am booting linux from sd card.  Can you please help me resolve this error.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,894件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi KENIZ

 

from log "Unable to handle kernel NULL pointer dereference" reason may be in wrong image.

One can reprogram image using Demo Image from link

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

use guidelines included in Linux Guide.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,895件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi KENIZ

 

from log "Unable to handle kernel NULL pointer dereference" reason may be in wrong image.

One can reprogram image using Demo Image from link

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

use guidelines included in Linux Guide.

 

Best regards
igor

0 件の賞賛
返信