Problems building ltib (elftosb missing)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems building ltib (elftosb missing)

Jump to solution
3,105 Views
dafmulder
Contributor I

Hello there,

I've a serious problem building my ltib. (for an analogue of the imx53 qsb)

The problem is the elftosb-11.09.01.tar.gz.md5 package which is not available online anymore.

I already tried working my way around it by using the source package for imx6 which has a 10.0.01 version of elftosb but to no avail.

Maybe there is someone with this package still somewhere or a different approach to it.

Error:

Try elftosb-11.09.01.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz.md5:

16:42:21 ERROR 404: Not Found.

Try elftosb-11.09.01.tar.gz from the GPP

http://bitshrine.org/gpp/elftosb-11.09.01.tar.gz:

16:42:22 ERROR 404: Not Found.

Can't get: elftosb-11.09.01.tar.gz at ./ltib line 790.

Died at ./ltib line 1380.

traceback:

main::build_host_rpms:1380

  main::host_checks:1435

   main:542


Labels (1)
0 Kudos
Reply
1 Solution
2,205 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
2,208 Views
dafmulder
Contributor I

Thank you, I eventually got it working with the 12.04LTIB

0 Kudos
Reply
2,206 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply