Problems adding olsrd package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems adding olsrd package

2,328 Views
unaigonzalez
Contributor II

I have this error trying to add olsrd package:

plc@ubuntu:~/ltib$ sudo ./ltib -m prep -p olsrd.spec

[sudo] password for plc:

You should not be root when running ltib, do you really

want to continue ? y|N

y

Processing: olsrd

===================

/home/plc/ltib/dist/lfs-5.1/olsrd-0.5.6-r8.tar.gz/olsrd.spec does

not contain an entry for Name: at /home/plc/ltib/bin/Ltibutils.pm

line 188.

Died at ./ltib line 752.

traceback:

main::build_rpm:752

main::f_prep:992

main:560

Exiting on error or interrupt

Labels (1)
0 Kudos
Reply
2 Replies

2,107 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Unai,

I've never try to add Olsrd package, but packages need to be added from the host libraries to the ltibutil.pm, please check

Best image for iMX6 Sabre Lite Board ?

Also, instead of ltib you should try to move to Yocto BSP.

Hope this helps

Have a great day,
Alfredo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,107 Views
unaigonzalez
Contributor II

Hay Bio,

I was trying to add manually the packages, i follow this steps:

1. copy source in /opt/freescale/pkgs
2. create file source_name.md5
md5sum source_name > source_name.md5
3. create directory in <you_ltib_dir>dist/lfs-5.1/<you_package> and copy spec-file to it

After this you can use ltib for build package:
1. ./ltib -m prep -p package.spec
2. ./ltib -m scbuild -p package.spec
3. ./ltib -m scdeploy -p package.spec

But the posted erro appear and I am pretty lost

0 Kudos
Reply