Hello All!
Have i.MX 6Quad Freescale SabreSD with Android 4.3
I want to connect to SabreSD the wifi module RTL8723BS by SDIO.
The main problem is:
I configure everything according to the instructions, but unfortunately it is not going to build like a KO (module).
Step by step:
CONFIG_CFG80211=y
CONFIG_MAC80211_MESH=y
CONFIG_MAC80211=y
CONFIG_HOSTAP=y
CONFIG_RTL8723BS=m 2. vim device/fsl/{yourdevice}/BoardConfig.mk
BOARD_WIFI_VENDOR := realtek
ifeq ($(BOARD_WIFI_VENDOR), realtek)
WPA_SUPPLICANT_VERSION := VER_0_8_X
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
CONFIG_DRIVER_WEXT :=y
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_WLAN_DEVICE := rtl8723bs
#BOARD_WLAN_DEVICE := rtl8192du
#BOARD_WLAN_DEVICE := rtl8192ce
#BOARD_WLAN_DEVICE := rtl8192de
#BOARD_WLAN_DEVICE := rtl8723as
#BOARD_WLAN_DEVICE := rtl8723au
#BOARD_WLAN_DEVICE := rtl8189es
#BOARD_WLAN_DEVICE := rtl8192cu
#BOARD_WLAN_DEVICE := rtl8723bu
WIFI_DRIVER_MODULE_NAME := "wlan"
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/wlan.ko"
WIFI_DRIVER_MODULE_ARG := "ifname=wlan0 if2name=p2p0"
WIFI_FIRMWARE_LOADER := ""
WIFI_DRIVER_FW_PATH_STA := ""
WIFI_DRIVER_FW_PATH_AP := ""
WIFI_DRIVER_FW_PATH_P2P := ""
WIFI_DRIVER_FW_PATH_PARAM := ""
endif 3. Add android.hardware.wifi.direct.xml
PRODUCT_COPY_FILES += \
frameworks/native/data/etc/android.hardware.wifi.direct.xml:system/etc/permissions/android.hard
ware.wifi.direct.xml 4. init.xxx.rc
service rtw_suppl_con /system/bin/wpa_supplicant \
-ip2p0 -Dnl80211 -c /data/misc/wifi/p2p_supplicant.conf -e/data/misc/wifi/entropy.bin -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class main
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service rtw_suppl /system/bin/wpa_supplicant -iwlan0 -Dnl80211
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class main
disabled
oneshot 5. Set wifi.interface
PRODUCT_PROPERTY_OVERRIDES += \
wifi.interface=wlan0 6. Apply wifi_realtek.c
ifeq ($(BOARD_WIFI_VENDOR), realtek)
LOCAL_SRC_FILES += ../realtek/wlan/libhardware_legacy/wifi/wifi_realtek.c
else
LOCAL_SRC_FILES += wifi/wifi.c
endif 7. wpa_supplicant_8
ifeq ($(BOARD_WIFI_VENDOR), realtek)
L_CFLAGS += -DREALTEK_WIFI_VENDOR
L_CFLAGS += -DANDROID_P2P
L_CFLAGS += -DCONFIG_ANDROID_4_2_PERSISTENT_IOT
Endif
8. Adding or Selecting Target Platform
opt/kernel_imx/drivers/net/wireless/rtl8723bs/makefile
CONFIG_PLATFORM_FSL_IMX6Q = y
CONFIG_PLATFORM_I386_PC = n
CONFIG_PLATFORM_ANDROID_X86 = n
CONFIG_PLATFORM_ARM_S3C2K4 = n
CONFIG_PLATFORM_ARM_PXA2XX = n
CONFIG_PLATFORM_ARM_S3C6K4 = n
CONFIG_PLATFORM_MIPS_RMI
= n
CONFIG_PLATFORM_RTD2880B
= n
CONFIG_PLATFORM_MIPS_AR9132 = n
CONFIG_PLATFORM_MT53XX
= n
CONFIG_PLATFORM_RTK_DMP
= n
9. opt/kernel_imx/drivers/net/wireless/Makefile
obj-$(CONFIG_RTL8723AS) += rtl8723as/10. opt/kernel_imx/drivers/net/wireless/Kconfig
source "drivers/net/wireless/rtl8723bs/Kconfig"The build is building success, but i don't get the KO module file in opt/out/target/product/sabresd_6dq/system/lib/module/
Thank's a lot for any help or ideas!
For now i have :
If i set in vim device/fsl/{yourdevice}/BoardConfig.mk
BOARD_WIFI_VENDOR := realtekBuiding success, but i don't get the KO module file.
if i set
BOARD_WLAN_VENDOR := realteki get error
make: *** No rule to make target `NOTICE-TARGET-STATIC_LIBRARIES-lib_driver_cmd_rtl', needed by `out/target/product/sabresd_6dq/system/bin/hostapd'. Stop.
make: *** Waiting for unfinished jobs....
for RALINK and ATHEROS ar6003 is set like WLAN, but in documentation for RTL8723BS is set WIFI.
What correct wlan or wifi?
if correct WLAN, why i get "No rule to make target `NOTICE-TARGET-STATIC_LIBRARIES-lib_driver_cmd_rtl'"
Hi Ma
RTL8723 is not nxp product and not supported in nxp linux bsp releases.
It is pure linux problem with building driver. As a rule, chip vendors (realtek in this case) are
providing documentation for porting drivers for their products. Seems most appropriate
way to apply to realtek support:
Best regards
igor
Again!!!!!! why my post is marked "CONSIDERS SOLVED" ???? NOT SOLVED!!!!
Stop to mark my quastions solved or CONSIDERS SOLVED.
This is misleading people. You find the question in the search, you think there is a solution. And here it is not!
There were gathered people who know how to use the search and read the documentation, asking the question they want to get help, not excuses.
Hi Ma
I am afraid you are not right, even people know how to use the search and
read the documentation, it is difficult for them to sort out correct search result and
interpret documentation. For many people often it is not easy to find
necessary document and explanations in it.
Please note that this forum is devoted to nxp i.mx processors and generic
linux questions not related to i.mx may be answered on generic linux forums.
Flag "Considered solved" does not mean that issue is solved. There is another
flag : "Correct answer" meaning that issue is solved. Flag "Considered solved"
means that was provided best available answer.
Please note that NXP has special service for providing support with customer
software porting: Professional Services
Best regards
igor
igorpadykov написал(а):
Flag "Considered solved"
means that was provided best available answer.
Who decided that this is the best answer?
I do not consider him the best. The best answer is when they give an answer or help with an excerpt from the code or from the documentation.. The best answer is not to redirect to another forum, redirect to "Professional Services" or read the documentation on page 55.
Entering to your profile,every one can see all the topics on which you "walked"
In each topic, you do not have a discussion on the problem, there is no excerpt from the code. You always simply indicate a link to the documentation or a similar topic "read there"
The best answer should be determined by the one who created the topic, and not the one who responded to it. You think in all topics your answers are the best, but this is not so and there is no help.
Hi Ma
as this is generic linux issue it could be posted on kernel mail list or
meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------