Problem with nand flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with nand flash programming

2,878件の閲覧回数
alessandrobenfe
Contributor I

Hi, i work with two SOM one with imx6solo and other one with imx6quad, both SOM have with same nand flash.

With a MicroSD card update the SOM; with imx6quad I always have success, but with imx6solo sometimes don't have success.

For update the rootfs I use a script with this instructions:
ubiformat -y /dev/mtd3
ubiattach /dev/ubi_ctrl -m 3
ubimkvol /dev/ubi0 -N rootfs -s445000000
mkdir /rootfs
mount -t ubifs ubi0:rootfs /rootfs
tar xvf /rootfs.tar.bz2 -C /rootfs
sync

When I boot from nand flash I have some errors of this type:

UBIFS error (ubi0:0 pid 277): ubifs_read_node: bad node type (255 but expected 1)
UBIFS error (ubi0:0 pid 277): ubifs_read_node: bad node at LEB 394:119808, LEB mapping status 0
Not a node, first 24 bytes:
00000000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ........................

I don't understand what the problem could be due to and what settings to check.

Note: I use a yocto pyro distribution

 

Can you help me?

Thanks,

Alessandro

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,769件の閲覧回数
kef2
Senior Contributor V

FF FF.. looks like erased flash page. It could be for example due to misconfigured U-Boot environment area in NAND flash, so that when U-Boot stores environment variables, NAND page(s) at bottom of your UBI partition gets erased.

0 件の賞賛
返信

2,773件の閲覧回数
alessandrobenfe
Contributor I

Hi,

from the tests carried out the error seems to occur due to the use of two different distributions of yocto to create the OS of the microSD and the one contained in the flash.

For the quad core version the same version of yocto was used for both the microSD and the flash.

I believe there is some incompatibility between the versions of the flash management drivers between the two kernel versions used in the yocto distributions.

At the moment, by using the same version of yocto to build the OS for everyone we solved the problem.

0 件の賞賛
返信

2,845件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check your SOM vendor because apparently t does not use the same nand on both MX6 processors.

Regards

0 件の賞賛
返信