Problem with linux-mfgtool and initramfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with linux-mfgtool and initramfs

2,585件の閲覧回数
erezamir
Contributor II

Hi,

I am trying to use kernel + initramfs provided with mfgtool package for SCM QWKS board.

I've managed to boot kernel via USB OTG but I get the following error:

request_module: runaway loop modprobe binfmt-0000

Failed to execute /linuxrc (error -8)

request_module: runaway loop modprobe binfmt-0000

Starting init: /bin/sh exists but couldn't execute it (error -8)

Kernel panic - not syncing: No working init found. Try passing........

I've tried to bitbake my own mfgtool uboot + linux + initramfs, with same result.

Please help to solve this.

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,164件の閲覧回数
marcooman
Contributor II

I am having a very similar problem with initramfs: the one built with yocto says

Failed to execute /linuxrc (error -80)

Starting init: /bin/sh exists but couldn't execute it (error -80)

0 件の賞賛
返信

2,164件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erez

please create service request to obtain additional documentation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信