Problem with interfacing SPI device with wandboard dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with interfacing SPI device with wandboard dual

1,972 Views
aravinds
Contributor I

Hi,
I'm using imx6 wandboard dual tried to configure spi1,

made device-tree changes:

-----------------------------------------------
...
&iomuxc {
...
    ecspi1 {
         pinctrl_ecspi1_cs: ecspi1cs {
                         fsl,pins = <
                             MX6QDL_PAD_EIM_EB2__ECSPI1_SS0  0x80000000
                             >;
                     };
 pinctrl_ecspi1: ecspi1grp {
                      fsl,pins = <
                          MX6QDL_PAD_EIM_D17__ECSPI1_MISO 0x100b1
                          MX6QDL_PAD_EIM_D18__ECSPI1_MOSI 0x100b1
                          MX6QDL_PAD_EIM_D16__ECSPI1_SCLK 0x100b1
                          >;
                  };
    };
...

...
&ecspi1 {
    fsl,spi-num-chipselects = <1>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi1 &pinctrl_ecspi1_cs>;
    status = "okay";
    spidev@0x01 {
        compatible = "linux,lcd-st7565";
        spi-max-frequency = <20000000>;
        reg = <0x0>;
        register-sel-gpio =<&gpio4 5 0>;
        reset-gpio =<&gpio7 13 0>;
        backlight-gpio =<&gpio3 26 0>;
        status = "okay";
    };
};
...
----------------------------------------------------------------

but while connecting the LCD to the SPI, its not working (lcd-st7565 driver for my LCD, which is working fine as i get all debug prints)on probing the SPI pins with oscilloscope confirmed data is coming but in some distorted manner (overshoot undershoot problem),

 

kernel version 3.14.28

oscilloscope probed  : data line and clock
can anyone please guide me what is the reason for such a behavior..??

Labels (3)
0 Kudos
Reply
1 Reply

1,721 Views
igorpadykov
NXP Employee
NXP Employee

Hi ARAVIND

lcd-st7565 driver should be integrated in linux framebuffer framework,

please follow  eLCDIF driver example described in Chapter 12 ELCDIF Frame Buffer Driver

attached Linux Manual. For debug testing one can use sect.6.4.1 Framebuffer Tests

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply