Problem with downloading FSL Yocto BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with downloading FSL Yocto BSP

跳至解决方案
4,246 次查看
xifan
Contributor II

Hi,

I am newbie in this field and have now problem with downloading FSL Yocto BSP in virtual machine Ubuntu Linux V14.04. the host system is Win7. I followed the guide: Freescale_Yocto_Project_User's_Guide.pdf.

- I am behind proxy server, but with the correct proxy settings, I can download and install the host packets successfully.

  (section 3.1 of the user's guide)

-  Following the section 3.2 I can setup the repo utility without any problem

After that I want to setup Yocto Project (section 4)

- I registered the git with the username and password

- generated the folder fsl-release-bsp

- At running the command repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga

  I get the following error messages:

/home/xfamed/bin/repo: line 1: html: No such file or directory

/home/xfamed/bin/repo: line 2: head: No such file or directory

/home/xfamed/bin/repo: line 3: title: No such file or directory

/home/xfamed/bin/repo: line 4: meta: No such file or directory

/home/xfamed/bin/repo: line 5: META: No such file or directory

/home/xfamed/bin/repo: line 6: meta: No such file or directory

/home/xfamed/bin/repo: line 7: style: No such file or directory

/home/xfamed/bin/repo: line 9: border:3px: command not found

/home/xfamed/bin/repo: line 9: $'\r': command not found

/home/xfamed/bin/repo: line 10: background-color:#fff: command not found

/home/xfamed/bin/repo: line 10: $'\r': command not found

/home/xfamed/bin/repo: line 11: margin:1.5em: command not found

/home/xfamed/bin/repo: line 11: $'\r': command not found

/home/xfamed/bin/repo: line 12: padding:1.5em: command not found

/home/xfamed/bin/repo: line 12: $'\r': command not found

/home/xfamed/bin/repo: line 13: font-family:Tahoma,Helvetica,Arial,sans-serif: command not found

/home/xfamed/bin/repo: line 13: $'\r': command not found

/home/xfamed/bin/repo: line 14: font-size:1em: command not found

/home/xfamed/bin/repo: line 14: $'\r': command not found

/home/xfamed/bin/repo: line 15: $'}\r': command not found

/home/xfamed/bin/repo: line 16: h1: command not found

/home/xfamed/bin/repo: line 17: font-size:1.3em: command not found

/home/xfamed/bin/repo: line 17: $'\r': command not found

/home/xfamed/bin/repo: line 18: font-weight:bold: command not found

/home/xfamed/bin/repo: line 18: $'\r': command not found

/home/xfamed/bin/repo: line 19: color:#196390: command not found

/home/xfamed/bin/repo: line 19: $'\r': command not found

/home/xfamed/bin/repo: line 20: $'}\r': command not found

/home/xfamed/bin/repo: line 21: b: command not found

/home/xfamed/bin/repo: line 22: font-weight:normal: command not found

/home/xfamed/bin/repo: line 22: $'\r': command not found

/home/xfamed/bin/repo: line 23: color:#196390: command not found

/home/xfamed/bin/repo: line 23: $'\r': command not found

/home/xfamed/bin/repo: line 24: $'}\r': command not found

/home/xfamed/bin/repo: line 25: /style: No such file or directory

/home/xfamed/bin/repo: line 26: /head: No such file or directory

/home/xfamed/bin/repo: line 27: body: No such file or directory

/home/xfamed/bin/repo: line 28: div: No such file or directory

/home/xfamed/bin/repo: line 29: h1: No such file or directory

/home/xfamed/bin/repo: line 30: p: No such file or directory

/home/xfamed/bin/repo: line 31: syntax error near unexpected token `<'

'home/xfamed/bin/repo: line 31: `<p><b>User:</b> 163.50.61.157 </p>

Could someone help me to find out the reason, why the repo init didn't work?

Some settings missing?

Thanks

Xi

0 项奖励
回复
1 解答
3,950 次查看
xifan
Contributor II

It is now resolved.

I delete the /bin/repo file, and run the following commands again:

mkdir ~/bin

curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

chmod a+x ~/bin/repo

git config --list (show me previously set name and email)

cd fsl-release-bsp

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga

after that I can do the repo initialization successfully.  repo sync runs then also without any problem.

Don't ask me why. There was something wrong with the first generation of repo file.

regards

Xi

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,951 次查看
xifan
Contributor II

It is now resolved.

I delete the /bin/repo file, and run the following commands again:

mkdir ~/bin

curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

chmod a+x ~/bin/repo

git config --list (show me previously set name and email)

cd fsl-release-bsp

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga

after that I can do the repo initialization successfully.  repo sync runs then also without any problem.

Don't ask me why. There was something wrong with the first generation of repo file.

regards

Xi

0 项奖励
回复
3,950 次查看
xifan
Contributor II

yes, it was/is executable (as section 3.3 described, I run the command chmod a+x ~/bin/repo) and using ls command I can verify it:

-rwxrwxr-x 1 xfamed xfamed 930 Jul 15 11:15 repo

Thanks

Xi

0 项奖励
回复
3,950 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following

https://community.nxp.com/message/809896?et=watches.email.thread#comment-809896

Regards,

Yuri.

0 项奖励
回复
3,950 次查看
xifan
Contributor II

Yuri,

thanks, I already resolved this problem: just remove the repo file, and then generate this repo file again.

I already updated this thread yesterday. Thanks a lot for your support!

BR

Xi

0 项奖励
回复
3,950 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please check if ~/bin/repo is (marked as) executable file

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复