Problem with disabling the MPLL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with disabling the MPLL

2,575 次查看
craighillis
Contributor I

When using a 26 MHz crystal, we can disable the MPLL to go to sleep mode. When the crystal is replaced with a 26 MHz oscillator, the MPLL is not reliably disabled.

The Reference manual states:

The conditions to be satisfied before the PLL Clock Controller actually turns off the MPLL are as

follows:

1. Clock Controller module has successfully mastered the system bus.

2. The A9P_CLK_OFF signal from the ARM9 Platform is active.

3. SDRAM controller has successfully placed the external SDRAM into Self-Refresh mode.

4. After the above conditions are satisfied, the countdown based on the value in the SD_CNT field

will be initiated.

5. SD_CNT countdown completes.

What could prevent the Clock Controller module from successfully mastering the system bus?

标签 (1)
0 项奖励
回复
6 回复数

2,382 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Craig

Clock Controller module may not successfully master the system bus

due to incorrect power-up sequence or external 26MHz clock noise /

noise on OSC26VDD, MPLLVDD power supplies. Note, external clock should

not be provided to unpowered processor, it should be applied along with

OSC26VDD power supply.  In general one can check low power mode sequence

by oscillosope outputting MPLL clock on CLKO pin with CCSR register or

check CKE signal with Figure 18-37. SDRAM/LPDDR Enter Self Refresh Mode

During System Sleep Mode i.MX27 RM.

Datasheet on p.28 recommends to disable oscillator circuit with CSCR (OSC26M_DIS)

and apply clock to EXTAL26M.  http://cache.freescale.com/files/dsp/doc/data_sheet/MCIMX27EC.pdf

External clock may not have the desired spectral purity, only a crystal will provide the necessary signal quality.

Below oscillator specs

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,382 次查看
craighillis
Contributor I

Igor,

Thanks for the reply.

Where can I find a specification on spectral purity and noise for the 26MHz oscillator?

According to the reference manual it can be a square wave.

When I first started looking at replacing the crystal with an oscillator I could not find any requirements for the i.MX27. A FAE at Avnet said to use the i.MX25 requirements.

Also, with regards to disabling the oscillator, we have tried that and the system does not run. In an earlier post you said:

Hi Chris

this bit can disable internal schematic, related to input 26MHz clock.

OSC26M_DIS = 1 disable 26MHz clock at all. This may be needed, say,

to decrease consumption when 26MHz clock is not used.

So, for any 26MHz configuration (crystal or generator) OSC26M_DIS

should be cleared.

Best regards

igor

Craig

0 项奖励
回复

2,382 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Craig

please create service request for providing

additional documents.

Best regards

igor

0 项奖励
回复

2,382 次查看
craighillis
Contributor I

How and where do I create a service request?

Craig

0 项奖励
回复

2,382 次查看
igorpadykov
NXP Employee
NXP Employee

To submit case  please follow below steps:

1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.

2) On the bottom of the page under Submit New Issues, click Hardware & Software.

3) Register with your business email to access NXP technical online support.

4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.

5) On the NXP online support page, select Contact Support from the top menu

and click ôsubmit a new caseö to start the process

~igor

0 项奖励
回复

2,382 次查看
craighillis
Contributor I

Thanks.

0 项奖励
回复