Problem with burn the NXP Linux BSP image to the 8MMini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with burn the NXP Linux BSP image to the 8MMini

3,053 Views
dong_tian
Contributor I

I download uuu and L4.14.98_2.0.0_ga_images_MX8MMEVK.zip in Ubuntu 18.04

and I burn L4.14.98_2.0.0_ga_images_MX8MMEVK.zip to 8MMini with cmd:

```

sudo uuu L4.14.98_2.0.0_ga_images_MX8MMEVK.zip

```

but it run and stopped as

```

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.91-0-g3799f4d

Success 0 Failure 0

1:2 3/ 3 [============100%============] SDPV: jump

```

I do above according to “Get Started with the i.MX 8M Mini EVK”[https://www.nxp.com/document/guide/get-started-with-the-i.mx-8m-mini-evk:GS-iMX-8M-Mini-EVK?lang=en&...]

but the linux cannot be burn into IMX 8MMini

It‘s anything wrong with this and what should I do?

0 Kudos
Reply
4 Replies

2,544 Views
walid_raach
Contributor I

I have the same problem with a custom board imx8mm,did you find the solution?the uuu is executable

U-Boot SPL 2018.03-4.14.98-2.2.0+g73af2fc (Dec 03 2019 - 17:03:27 +0000)
power_bd71837_init
DDRINFO: start DRAM init
DRAM PHY training for 1600MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 1377464 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image
Found header at 0x40435000


U-Boot 2018.03-4.14.98-2.2.0+g73af2fc (Dec 03 2019 - 17:03:27 +0000)

CPU:   Freescale i.MX8MMQL rev1.0 1600 MHz (running at 1200 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 39C
Reset cause: POR
Model: FSL i.MX8MM DDR3L Validation board
DRAM:  2 GiB
NAND:  0 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - ATF 1355c5d
  - U-Boot 2018.03-4.14.98-2.2.0+g73af2fc

switch to partitions #0, OK
mmc1(part 0) is current device
Net:   
Error: ethernet@30be0000 address not set.
No ethernet found.
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;booti ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Bad Linux ARM64 Image magic!
u-boot=>

Capture du 2019-12-04 09-10-40.png

0 Kudos
Reply

2,544 Views
dong_tian
Contributor I

I'm sorry to say that we have abandoned imx8mm. So we didn't find the solution.

0 Kudos
Reply

2,544 Views
dong_tian
Contributor I

There is the u-boot log

```

Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 1042272 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image

U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g654088c (Nov 28 2018 - 19:15:55 +)

CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Card did not respond to voltage select!
*** Warning - No block device, using default environment

Failed (-5)
No panel detected: default to MIPI2HDMI
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF d6451cc
- U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g654088c

Card did not respond to voltage select!
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee};
Hit any key to stop autoboot: 0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
g_dnl_register: failed!, error: -19
u-boot=>

```

0 Kudos
Reply

2,544 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Did you give executable permissions to the UUU tool?

Whit that, the download of the Linux into my board was successful.

Hope this information can help you.

Best regards,

Diego.

0 Kudos
Reply