Problem with booting from eMMC. Can't write u-boot correctly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with booting from eMMC. Can't write u-boot correctly

1,723件の閲覧回数
3dfxuser
Contributor I

Hello!

I've got a problem during getting eMMC boot work. I’ll say right away that this is definitely not the case of wrong fuses, GPIO settings or something else because everything worked fine until recently.

I followed this instruction, but system don't boot without any messages on UART. I think that this is related to the boot sector, since the control from the u-boot on SD card is successfully transferred to the system installed on the eMMC.

How can I get it work?  Will be appreciate for every help.

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,649件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alex

that link is third party resource developed and supported by solidrun,

one can post it on its forum: https://developer.solid-run.com/ 

NXP uses uuu tool for programming images

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Linux documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信