Problem with booting from eMMC. Can't write u-boot correctly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with booting from eMMC. Can't write u-boot correctly

1,737 Views
3dfxuser
Contributor I

Hello!

I've got a problem during getting eMMC boot work. I’ll say right away that this is definitely not the case of wrong fuses, GPIO settings or something else because everything worked fine until recently.

I followed this instruction, but system don't boot without any messages on UART. I think that this is related to the boot sector, since the control from the u-boot on SD card is successfully transferred to the system installed on the eMMC.

How can I get it work?  Will be appreciate for every help.

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,663 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

that link is third party resource developed and supported by solidrun,

one can post it on its forum: https://developer.solid-run.com/ 

NXP uses uuu tool for programming images

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Linux documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply