Problem with Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Yocto

1,481件の閲覧回数
alexberenshtein
Contributor III

mkdir fsl-release-bsp

cd fsl-release-bsp

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.0.xml

Get https://gerrit.googlesource.com/git-repo/clone.bundle Get https://gerrit.googlesource.com/git-repo remote: Finding sources: 100% (13/13) remote: Total 13 (delta 3), reused 13 (delta 3) Unpacking objects: 100% (13/13), done. From https://gerrit.googlesource.com/git-repo 35d2221..259f165 master -> origin/master Get git://git.freescale.com/imx/fsl-arm-yocto-bsp.git fatal: unable to connect to git.freescale.com: git.freescale.com[0: 192.88.156.202]: errno=Connection timed out fatal: unable to connect to git.freescale.com: git.freescale.com[0: 192.88.156.202]: errno=Connection timed out

ラベル(3)
0 件の賞賛
返信
1 返信

1,236件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Alex,

When 'repo init' process is completed, the source code is checked out into the directory <BSP-Directory>/sources. A successful initialization will end with a message stating that Repo is initialized in your working directory. Your client directory should contain a hidden .repo directory where files such as the manifest will be kept.

First you may update and upgrade your host machine. If errors occur during repo initialization, try deleting the .repo directory and running the repo initialization command again.


If the problems persists verify that you have internet connection and you may contact your system administrator because if you are using firewalls or porxy server this may avoid conenction to repo.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信