Dear All,
My customer has planned the Digital Signage product using i.MX6 SoloLite.
They will use 24bit 1280 x 800 LCD.
I checked the data sheet and reference manual for SoloLite.
And I have found that there is a description which is different in each.
DS: Page 4.
LCD, 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60 Hz)
RM: Page 131.
  LCDIF supporting one parallel 24-bit LCD display with up to WXGA(1366x768)
  resolution at 60 Hz
Which is correct?
BR,
George
解決済! 解決策の投稿を見る。
Hi George
correct is 1366x768. However there is no hardware restriction on size and
with 1280 x 800 it also will work fine, but with less fps.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi George
correct is 1366x768. However there is no hardware restriction on size and
with 1280 x 800 it also will work fine, but with less fps.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------