Problem with MFGTool2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with MFGTool2

2,061件の閲覧回数
marcelballmann
Contributor III

Hi,

I have a SABRE-SD board with a iMX6Q. I have connect the USB port OTG and have done the changes from the chapter 3.3 of the Android Quick Start Guide, Rev jb4.2.2_1.0.0-GA, 05/2013.

But when I want to start the exe at point 7 of the Guide, I get a error message and no MfgTool opens. And the messages in the log do not help me, maybe you. The log file you can find attached. Thank you....

Original Attachment has been moved to: MfgTool.log.zip

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,756件の閲覧回数
jam
Contributor I

Change the name of the u-boot file that the instructions tell you to use to "u-boot."

0 件の賞賛
返信

1,756件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Marcel,

Did you try to open MFGTool before you did changes to the files?, what changes did you do to UCL2.xml?