Problem with GC320 (2D Composition)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with GC320 (2D Composition)

10,332 Views
ali_sarlak
Contributor III

Hello community,

Is there any sample codes, examples, etc that using GC320 (2D Composition) on IMX6Q?

Especially for using overlay feature ,I don't know I've to use (i.MX 6 2D API) or (Directfb1.4.0) ...???

I've searched a lot but no luck!

I appreciate any idea.

Regards,

Ali

0 Kudos
Reply
2 Replies

9,913 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look at sect.8.2 G2D-fsl-samples attached Linux Guide

and

About G2D API in i.MX6DQ.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,913 Views
ali_sarlak
Contributor III

Hi igorpadykov,

I've read the sect.8.2 that's about 2D API, can I use overlay feature with 2D API or I've to use something else?

In another post https://community.nxp.com/thread/395688 your college suggests me to use Wayland in order to deal with GC320 and overlay feature.

Could you please clarify it for me which API (Wayland, G2D, HAL2D,DirectFB,...) should I use?

Regards,

Ali

0 Kudos
Reply