Problem using external clock on DI0 with parallel interface LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem using external clock on DI0 with parallel interface LCD

2,650件の閲覧回数
muzammalahmed
Contributor I

Hi,

I'm trying to use an external clock on DI0 (DI0_EXT_CLK) for parallel LCD. When I do this, I see the last line on my display flashes bright white. It is always the last line and flashes frequently without fixed timeframe. I do not see this problem when I use internal clock. Has anyone ran into this issue? Is there a way to synchronize IPU clock (HSP_CLK) and DI external clock (DI0_EXT_CLK)? Why don't I see this issue when I use internal clock? Is there something else I need to do besides setting di0_ext_clk bit in ipu_di0_general register?

Thanks,

ラベル(2)
3 返答(返信)

2,275件の閲覧回数
YixingKong
Senior Contributor IV

The issue will be closed if there is no response in 3 days.

0 件の賞賛
返信

2,275件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support
Re: Problem using external clock on DI0 with parallel interface LCD

Rogerio NunesEmployee

I think I got this same question from Ahmed through the Sales team in December.

He was using an i.MX53 and his external clock frequency was higher than 90% of 200Mhz (maximum IPU clock frequency). I suggested trying an external clock with lower frequency.

0 件の賞賛
返信

2,275件の閲覧回数
Ragan_Dunham
NXP Employee
NXP Employee

Muzammal,

Since this issue is a bit stale can you please let me know if in fact it is still open on your side?  If so is there any updated progress to report?  Let me know and I'll have someone take a look.

Thanks,

Ragan

0 件の賞賛
返信