Problem loading u-boot image after updating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem loading u-boot image after updating

1,459件の閲覧回数
jfg
Contributor I

Hi,

I have an older u-boot version (imx_v2009.08_3.0.35_4.1.0 877fd9eea1858585c8939e05173feb612c42a95f) running our custom board (similar to imx6dlsabresd).

Now i'm trying to update u-boot to the imx_v2014.04_3.10.53_1.1.0_ga version. I have followed the "i.MX 6 BSP Porting Guide, Rev. L3.10.53_1.1.0-ga, 01/2015" and I used mx6sabresd as a base and added my old dcd table to that. I compiled and used MFG-tool (imx-3.10.53_1.1.0_ga-mfg-tools) to load the image to the board. However the board doesn't seem to boot correctly, when checking the settings with jtag I can see that the dcd table hasn't loaded correctly. I compiled this stand-alone without yocto and used Sourcery CodeBench Lite 2012.09-64 4.7.2

 

Any clues on what could be wrong would be very helpful.

Original Attachment has been moved to: ucl2.xml.zip

Original Attachment has been moved to: dcd_table.cfg.zip

タグ(3)
0 件の賞賛
返信
1 返信

1,307件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Johan

had you tried to change only uboot../mx6sabresd/mx6dlsabresd.cfg

with new ddr settings?

Best regards

igor

0 件の賞賛
返信