Problem in running LTIB..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in running LTIB..

6,043件の閲覧回数
jagadeeshv
Contributor II

Hi all,

I'm new one to LTIB...

i've followed instructions from some forums and sites to DL & run LTIB..

i've stopped at "wget-ssl" & "rpm build"

*********************************************************

Processing platform: Host support packages

============================================

using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig

Processing: fake-provides

===========================

Processing: mkspooflinks

==========================

Processing: distcc

====================

Processing: ccache

====================

Processing: bison

===================

Processing: flex

==================

Processing: texinfo

=====================

Processing: autoconf

======================

Processing: libtool

=====================

Processing: lkc

=================

Processing: patch

===================

Processing: wget-ssl

======================

Build path taken because: no prebuilt rpm,

rpmbuild --dbpath ///opt/ltib/var/lib/rpm --target i686 --define '_unpackaged_files_terminate_build 0' --define '_target_cpu i686' --define '__strip strip' --define '_topdir /opt/ltib/usr/src/rpm' --define '_prefix /opt/ltib/usr' --define '_tmppath /home/jag/Desktop/ltib/tmp' --define '_rpmdir /opt/ltib/usr/src/rpm/RPMS'  --define '_mandir /opt/ltib/usr/share/man' --define '_sysconfdir /opt/ltib/etc' --define '_localstatedir /var' -bb --clean --rmsource  /home/jag/Desktop/ltib/dist/lfs-5.1/wget/wget-ssl.spec

.

.

.

.

.

checking for libgnutls... no

configure: error: --with-ssl was given, but GNUTLS is not available.

error: Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.13495 (%build)

RPM build errors:

    Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.13495 (%build)

Build time for wget-ssl: 48 seconds

Failed building wget-ssl

Died at ./ltib line 1492.

traceback:

main::build_host_rpms:1492

  main::host_checks:1554

   main:562

Started: Sun Sep 14 02:07:47 2014

Ended:   Sun Sep 14 02:08:35 2014

Elapsed: 48 seconds

VERSION          : 13.2.1

CVS_VERSION      : $Revision: 1.93 $ (Savannah)

PLATFORM         : host

GNUTARCH         : i686

TOOLCHAIN        :

TOOLCHAIN_CFLAGS :

These packages failed to build:

wget-ssl

Build Failed

*****************************************

I've tried all fixes got from net...

but i'm unable to run LTIB on my PC...

I've installed Ubuntu 10.04 in my VMplayer..

please suggest me solution..

thanQ in advance...!!!!!!

ラベル(1)
11 返答(返信)

5,459件の閲覧回数
jagadeeshv
Contributor II

Hi All,

after all I've compiled and run LTIB on my PC..

but this time i got another source from friend, which is 1.3GB tar file,

now i got all required libraries and sources are with in the tar file,

"L3.0.35_4.1.0_130816_source.tar".....

Now no issues in running and using LTIB...

thankyou all.....

0 件の賞賛
返信

5,459件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I would recommend you to use Yocto instead. You will probably be up and running quicker.

5,459件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jagadeesh,

Which board and BSP are you using?
Have a great day,
(Dan)

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,459件の閲覧回数
jagadeeshv
Contributor II

HI Dan,

for Just now my task is to run LTIB successfully on my PC....

after that i'll use it for iMX6sl...

now is that matter of "BSP"....???

0 件の賞賛
返信

5,459件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jagadeesh,

No, I mean which version  BSP you are using so that I can give you the user guide document. As you have installed the LTIB on your PC, and the next step is to build the BSP using LTIB.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,459件の閲覧回数
jagadeeshv
Contributor II

Hi Dan,

did you got the  correct answer for the BSP version.... ??

i need some help... urgent..

I've installed LTIB .. following these instructions from the below link....

LTIB : Download

and installed the required packages...

thanks in advance...!!

5,459件の閲覧回数
jagadeeshv
Contributor II

hi Dan,

my ubuntu configuration ....

jag@ubuntu:~$ uname -a

Linux ubuntu 2.6.32-66-generic #132-Ubuntu SMP Mon Sep 1 18:36:19 UTC 2014 i686 GNU/Linux

jag@ubuntu:~$

thanks in advance...

0 件の賞賛
返信

5,459件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

5,459件の閲覧回数
jagadeeshv
Contributor II

Hi Luis Casado...

I've followed the above two links...

and installed all patches suggested by them...

after running LTIB a got this log....

*******************************************

Processing platform: Host support packages

============================================

using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig

Processing: fake-provides

===========================

Processing: mkspooflinks

==========================

Processing: distcc

====================

Processing: ccache

====================

Processing: bison

===================

Processing: flex

==================

Processing: texinfo

=====================

Processing: autoconf

======================

Processing: libtool

=====================

Processing: lkc

=================

Processing: patch

===================

Processing: wget-ssl

======================

Build path taken because: no prebuilt rpm,

Use of uninitialized value in string eq at /home/jag/Desktop/ltib/bin/Ltibutils.pm line 370.

Try wget-1.14-perl5.18-fix.patch.md5 from the GPP

http://bitshrine.org/gpp//wget-1.14-perl5.18-fix.patch.md5:

2014-09-15 08:59:36 ERROR 404: Not Found.

Use of uninitialized value in string eq at /home/jag/Desktop/ltib/bin/Ltibutils.pm line 370.

Try wget-1.14-perl5.18-fix.patch from the GPP

http://bitshrine.org/gpp//wget-1.14-perl5.18-fix.patch:

2014-09-15 08:59:37 ERROR 404: Not Found.

Can't get: wget-1.14-perl5.18-fix.patch at ./ltib line 790.

Died at ./ltib line 1380.

traceback:

main::build_host_rpms:1380

  main::host_checks:1435

   main:542

Started: Mon Sep 15 08:59:35 2014

Ended:   Mon Sep 15 08:59:37 2014

Elapsed: 2 seconds

These packages failed to build:

wget-ssl

Build Failed

*******************************************

for wget-ssl building error... all are suggested that .." include --without-ssl " in ./config line in this path  dist/lfs-5.1/wget/wget.spec

but this is already exist... in that line..

I'm unable to run this....

thanQ.. n suggest me how to build correctly...

0 件の賞賛
返信

5,459件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Your build fails because some packages are not found in bitshrine.org

ERROR 404: Not Found.

But I don't know why that patch should be needed, as LTIB builds wget-1.9.1.tar.gz that you should have in /opt/Freescale/pkgs

What is the BSP you're installing?

Luis

0 件の賞賛
返信

5,459件の閲覧回数
jagadeeshv
Contributor II

Hi Luis,

previously... I run some scripts from some other forum... so i got them..

now i've cleared all those things and run the LTIB again...

i got struced again in processing wget-ssl...

the log is here..

***************************************************

Processing platform: Host support packages

============================================

using /home/jag/Desktop/ltib/config/platform/host/ltib.preconfig

Processing: fake-provides

===========================

Processing: mkspooflinks

==========================

Processing: distcc

====================

Processing: ccache

====================

Processing: bison

===================

Processing: flex

==================

Processing: texinfo

=====================

Processing: autoconf

======================

Processing: libtool

=====================

Processing: lkc

=================

Processing: patch

===================

Processing: wget-ssl

======================

Build path taken because: directory build, no prebuilt rpm,

Cowardly refusing to clobber existing directory:

/opt/ltib/usr/src/rpm/BUILD/wget-1.14

Remove this by hand if you really want to rebuild this package from scratch

Died at ./ltib line 1492.

traceback:

main::build_host_rpms:1492

  main::host_checks:1554

   main:562

Started: Sat Sep 27 10:35:30 2014

Ended:   Sat Sep 27 10:35:30 2014

Elapsed: 0 seconds

VERSION          : 13.2.1

CVS_VERSION      : $Revision: 1.93 $ (Savannah)

PLATFORM         : host

GNUTARCH         : i686

TOOLCHAIN        :

TOOLCHAIN_CFLAGS :

These packages failed to build:

wget-ssl

Build Failed

***************************************************

i'm new one to the LTIB and want run LTIB on my PC (UBUNTU 10.04)...
if I pass in that i'll get work for iMX6SL......

so please help me to set this....

got this log after removing wget.spec..

.

.

.

.

checking for compress in -lz... (cached) yes

checking for gpg_err_init in -lgpg-error... no

checking for gcry_control in -lgcrypt... no

checking for libgnutls... no

configure: error: --with-ssl was given, but GNUTLS is not available.

error: Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.87523 (%build)

RPM build errors:

    Bad exit status from /home/jag/Desktop/ltib/tmp/rpm-tmp.87523 (%build)

Build time for wget-ssl: 37 seconds

Failed building wget-ssl

Died at ./ltib line 1492.

traceback:

main::build_host_rpms:1492

  main::host_checks:1554

   main:562

Started: Sat Sep 27 10:46:20 2014

Ended:   Sat Sep 27 10:46:57 2014

Elapsed: 37 seconds

VERSION          : 13.2.1

CVS_VERSION      : $Revision: 1.93 $ (Savannah)

PLATFORM         : host

GNUTARCH         : i686

TOOLCHAIN        :

TOOLCHAIN_CFLAGS :

These packages failed to build:

wget-ssl

Build Failed

***************************

please help me to fix this....

thanks in advance..

0 件の賞賛
返信