Problem in loading kernel image in imx6sl.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in loading kernel image in imx6sl.

Jump to solution
3,406 Views
pinkisaharan
Contributor II

Hi All,

I am using imx6SL board and when i am booting the board with linux image through MMC, i am getting the error:

Saving Environment to MMC...

Writing to MMC(1)... done

MX6Sl EVK U-Boot > boot

Card did not respond to voltage select!

mmc2(part 0) is current device

MMC read: dev # 2, block # 2048, count 8192 ... Card did not respond to voltage select!

MMC: block number 0x2800 exceeds max(0x0)

0 blocks read: ERROR

Can anyone help me with this..

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,533 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Pinki

     Can you try using mmc dev 0?

     I just tried on my EVK board, it is OK. After boot up uboot, type "mmc dev 0", then "mmc read 80800000 800 8000", then "bootm", kernel is booting up.

     BTW, my uImage is in SD card, and I boot from SD1.

     I guess your problem is that, you select a wrong mmc dev. If "mmc dev 0" did NOT work, try "mmc dev 1" or "mmc dev 2".

View solution in original post

0 Kudos
Reply
2 Replies
2,533 Views
felipezimmerle
Contributor II

Dear Pinki,

I've been facing the exactly same problem, whenever i use a micro-SD + SD adapter this happens. I am bypassing this, by interrupting the u-boot process at the debug console and asking the device to reset.

Repeat this process three times and it will work like a charm. You just need to do this when power up the device, after power up, reboots went just fine.

--

F.

0 Kudos
Reply
2,534 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Pinki

     Can you try using mmc dev 0?

     I just tried on my EVK board, it is OK. After boot up uboot, type "mmc dev 0", then "mmc read 80800000 800 8000", then "bootm", kernel is booting up.

     BTW, my uImage is in SD card, and I boot from SD1.

     I guess your problem is that, you select a wrong mmc dev. If "mmc dev 0" did NOT work, try "mmc dev 1" or "mmc dev 2".

0 Kudos
Reply