Problem in getting Android source code from Google repo as per i.MX Android r9.3 User Guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in getting Android source code from Google repo as per i.MX Android r9.3 User Guide

1,929件の閲覧回数
admin
Specialist II

I

As specified in the

i.MX Android R9.4 User Guide

in section

2. Build Android for i.MX

2.1 Get Android Source Code (Android/Kernel/U-Boot)

While getting the Android source code from Google repo, wen i was executing the  following step:


ubuntu@ubuntu-laptop:~/myandroid$ ./repo init -u git://android.git.kernel.org/platform/manifest.git -b android-2.2.1_r1

 

I was facing the below problem while downloading the android-2.2.1_r1 in the terminal window  of ubuntu


Getting manifest ...
   from git://android.git.kernel.org/platform/manifest.git
android.git.kernel.org[0: 149.20.4.77]: errno=Connection refused
fatal: unable to connect a socket (Connection refused)
fatal: cannot obtain manifest git://android.git.kernel.org/platform/manifest.git
ubuntu@ubuntu-laptop:~/myandroid$

 

Could ne body pls kindly do the needful in resolving the above issue so that i can proceed further

 

ne help would be greatly appreciated

 

Awaiting for your replies

Thanks!

Srinivasan

mail id:[email protected]

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,837件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

http://imxcommunity.org/forum/topics/problem-getting-android-source-kernel-source-from-kernel-org?co...

 

sorry for my mistake

 

you're trying a different release, but it should work with small change

0 件の賞賛
返信

1,837件の閲覧回数
admin
Specialist II

The below link is directing me to the same link which u replied, could u please resend the the exact link wher i can get the exact procedure for overcming my previous issues

http://imxcommunity.org/forum/topics/problem-in-getting-android-source-code-from-google-repo-as-per-...

 

kindly helpme,

Srinivasan S

0 件の賞賛
返信

1,837件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee
0 件の賞賛
返信