Problem in finding gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in finding gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12

ソリューションへジャンプ
3,716件の閲覧回数
sudiptasubudhi
Contributor III

Hello, I am using IMX6 board for porting of GPU applications for which i require this toolchain : gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12. As per my search, it should be found in Latest linux BSPs provided by freescale but i do not know which release of linux contains this and if it is present, i want to know the path in that BSP. could anyone please help me with it? Thanks in advancePr

1 解決策
2,367件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please use "gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm",

that may be found in pkgs directory of "L3.0.35_4.1.0_130816_source.tar.gz"

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_ER_SOURCE_BSP&appType=license&locati...

Summary Page :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,368件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please use "gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm",

that may be found in pkgs directory of "L3.0.35_4.1.0_130816_source.tar.gz"

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_ER_SOURCE_BSP&appType=license&locati...

Summary Page :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,367件の閲覧回数
davidjonathan
Contributor I

Do you know where I can find the glibc-2.13 source used to build the libraries that are part of that RPM?  I need to patch the libresolv code to fix the recently discovered getaddrinfo() problem (https://sourceware.org/ml/libc-alpha/2016-02/msg00416.html ).

The glibc source is not included in that RPM, nor AFAIK in the L3.0.35_4.1.0_130816_source.tar.gz tarball.

Thanks.

-David

0 件の賞賛
返信
2,367件の閲覧回数
sudiptasubudhi
Contributor III

Thank you Yuri

0 件の賞賛
返信