Problem in copying rootfs image through UUU tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in copying rootfs image through UUU tool

Jump to solution
2,042 Views
kmagi
Contributor III

Hi All,

I am facing an issue with burning the rootfs on NAND through UUU tool.

The script has below entries for burning kernel, dtb and rootfs,

# Create a mount point
FBK: ucmd mkdir -p /mnt/mountpoint

# burn kernel + device tree
FBK: ucmd mount -t ubifs ubi0:kernel1 /mnt/mountpoint
FBK: ucp zImage t:/mnt/mountpoint/zImage.bin
FBK: ucp imx6ull-14x14.dtb t:/mnt/mountpoint/imx6ull-14x14.dtb
SDP: delay 1000
FBK: ucmd umount /mnt/mountpoint


# burn rootfs
FBK: ucp ev-production-image-imx6ull.squashfs t:/tmp/ev-production-image-imx6ull.squashfs
FBK: ucmd ubiupdatevol /dev/ubi0_1 /tmp/ev-production-image-imx6ull.squashfs

 

When the script is run, it pass through kernel and dtb burning on NAND successfully but fails to copy the rootfs image into local /tmp directory

1:1>Start Cmd:FBK: ucmd mkdir -p /mnt/mountpoint
1:1>Okay (0.034s)
1:1>Start Cmd:FBK: ucmd mount -t ubifs ubi0:kernel1 /mnt/mountpoint
1:1>Okay (0.31s)
1:1>Start Cmd:FBK: ucp zImage.bin t:/mnt/mountpoint/zImage.bin
100%1:1>Okay (0.429s)
1:1>Start Cmd:FBK: ucp imx6ull-14x14.dtb t:/mnt/mountpoint/imx6ull-14x14.dtb
205%1:1>Okay (0.006s)
1:1>Start Cmd:FBK: ucmd umount /mnt/mountpoint
1:1>Okay (3.303s)
1:1>Start Cmd:FBK: ucp ev-production-image-imx6ull.squashfs t:/tmp/ev-production-image-imx6ull.squashfs
92%1:1>Fail (3.286s)
 
The rootfs file size is around 67MB and my DRAM size is 256MB.
Any feedback is appreciated.
 
Regards,
Kiran
0 Kudos
Reply
1 Solution
2,016 Views
kmagi
Contributor III

Finally, I am able to solve the problem by using the other partition "/none" which i don't know why it is created. I suppose it is for general development purpose.

none 95M 0 95M 0% /dev

Thanks

View solution in original post

0 Kudos
Reply
3 Replies
2,017 Views
kmagi
Contributor III

Finally, I am able to solve the problem by using the other partition "/none" which i don't know why it is created. I suppose it is for general development purpose.

none 95M 0 95M 0% /dev

Thanks

0 Kudos
Reply
2,019 Views
kmagi
Contributor III

Hello @Zhiming_Liu ,

 

The uuu.auto script doesn't helped much.

I checked that the ramfs size before the copy of my rootfs and it shows that the available memory is 61M and my rootfs size is 67M that is why it failed at 92% because the ramfs size is getting full.

1:2>Start Cmd:FBK: ucmd df -h
Filesystem Size Used Avail Use% Mounted on
rootfs 95M 34M 61M 36% /
none 95M 0 95M 0% /dev
1:2>Okay (0.02s)
 
How can I increase the ramfs size?
 
Thanks,
Kiran
0 Kudos
Reply
2,031 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

You can refer to uuu.auto in demo image

 

BR

Zhiming

 

0 Kudos
Reply