Problem import project fro imx93 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem import project fro imx93 evk

1,404 Views
geb
Contributor III

Hi,

I have a problem to import e project that we have modified that is the hello world for use it for try to change color to the rgb pwm led but when I try to import it says invalid CMake project archive, there is the possibility to resolve this problem?

problem import poject.PNG

 Thanks

0 Kudos
Reply
4 Replies

1,345 Views
geb
Contributor III

Hi @Chavira ,

The external project is imported now, but it's say that can't debug because can't crate a cmake build why?

Thanks

0 Kudos
Reply

1,381 Views
geb
Contributor III

Hi @Chavira ,

I'm using MCUXPRESSO extention to import a project, but not from the demo, I have imported a project that we have modified but when I try to debug it says that cn't debug because can't crate a cmake build why?

Thank & Regards

0 Kudos
Reply

1,372 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @geb!

You can import a local project too.

Chavira_0-1738086868832.png

 

I have tried without problems.

Chavira_1-1738087051740.png



You have to select the toolchain and the sdk path.

 

0 Kudos
Reply

1,393 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @geb!

Thank you for contacting NXP Support!

 

You should use the MCUXPRESSO extention to import a project:

Chavira_0-1737999429431.png

 

Best Regards!

Chavira

0 Kudos
Reply