Problem debug MCUxpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem debug MCUxpresso

2,019 Views
michelet1
Contributor II

Hello everybody,

Lately a strange error came out using MCUxpresso 11.6.1[build 8255]

The error happens when i run debugging using LPC-LINK2.

error is as follow:

/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-338_20211018_1634516203/src/gdb/gdb/utils.c:671: internal-error: virtual memory exhausted: can't allocate 4064 bytes.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Quit this debugging session? (y or n) [answered Y; input not from terminal]

This is a bug, please report it. For instructions, see:
<https://www.gnu.org/software/gdb/bugs/>.

/mnt/workspace/workspace/GCC-10-pipeline/jenkins-GCC-10-pipeline-338_20211018_1634516203/src/gdb/gdb/utils.c:671: internal-error: virtual memory exhausted: can't allocate 4064 bytes.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Create a core file of GDB? (y or n) [answered Y; input not from terminal]

 

I can't figure out how to deal with this problem, i didn't find any possible solution on NXP doc.

Thanks in advance to anyone who can help me

0 Kudos
Reply
2 Replies

2,002 Views
michelet1
Contributor II

Anyone have any ideas on what could be causing this anomalous behavior?

0 Kudos
Reply

1,991 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I suggest you try to update the firmware, I find this document maybe could help you with the steps.

LPC-Link2 Debug Probe Firmware Programming (nxp.com)

Best regards,
Pavel

0 Kudos
Reply