Problem about GPU's __ResetGPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem about GPU's __ResetGPU

2,271 Views
jiongzhongliu
Contributor III

My board is a custom board based on IMX6Q sabresd,I used linux 3.10(yocto git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.2_ga)。I shall use this linux version.

there is a problem about GPU initialization,it initialize the GPU failed, and I found it is hang in gc_hal_kernel_hardware.c--->__RestGPU:

static gceSTATUS _ResetGPU(

    IN gckHARDWARE Hardware,

    IN gckOS Os,

    IN gceCORE Core

    )

{

.......

    for (;;)

    {

        ....

        gcmkONERROR(gckOS_WriteRegisterEx(Os,

                                          Core,

                                          0x00000,

                                          control));

        /* Read idle register. */

        gcmkONERROR(gckOS_ReadRegisterEx(Os,

                                         Core,

                                         0x00004,

                                         &idle));

        if ((((((gctUINT32) (idle)) >> (0 ? 0:0)) & ((gctUINT32) ((((1 ? 0:0) - (0 ? 0:0) + 1) == 32) ? ~0 : (~(~0 << ((1 ? 0:0) - (0 ? 0:0) + 1)))))) ) == 0)

        {

            continue;      -------------------------------------->( **************always continue there*********)

        }

        .....

    }

.....

}

It seems  the write register failed. Can any body tell me what cause this problem? thank you!

Labels (2)
0 Kudos
Reply
3 Replies

2,105 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

you can narrow down issue, if this is caused by DDR errors or some

gpu erratum, running codes on reference Sabre board or using

more new linux where many gpu errata were fixed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,105 Views
jiongzhongliu
Contributor III

thank you. Is there a datasheet about IMX6Q's GPU registers? The IMX6Q datasheet describe nothing about GPU registers.

0 Kudos
Reply

2,105 Views
igorpadykov
NXP Employee
NXP Employee

unfrotunately no, as this is confidential info.

0 Kudos
Reply