Pro audio signal processing + AVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pro audio signal processing + AVB

1,779件の閲覧回数
farhadgholami
Contributor I

Hello We are looking to implement professionl audio signal processing  at the AVB end point (32 bits audio samples) athe AVB endpoit .

We want to implemen   multi channel audio filtering/signal processing (fixed point or floating point).

Dose current hardware /software stack suppports this?

0 件の賞賛
返信
2 返答(返信)

1,699件の閲覧回数
art
NXP Employee
NXP Employee

From the hardware point of view, it is possible to implement the task you describe on i.MX6 series processors, since they support IEEE 1588 timestamping feature in hardware, provide a number of digital audio interfaces and enough computing performance.

Regarding the software, no special audio processing applications are provided. The AVB stack software exists, but it is not for free, please contact the NXP Professional Services for more details:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,699件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Farhad,

NXP offers the complete AVB Stack but it is not for free you can contact our  Professional Services.  Here is a Link to get a qoute:

NXP Professional Services|NXP


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信