Hi,
We're using i.MX6QP processor to communicate with the external LCD display through LVDS-Bridge interface. But LVDS Bridge seems to be more like a buffer, which simply transmits Differential-ended signals to the display unit. I would like to understand really which peripheral (inside i.MX) is responsible for handling the display unit. And please provide the details of communication protocol between the display and that peripheral. Basic documents, if any, helpful for understanding the processing between that peripheral and the display unit are most welcome to be shared.
My Basic requirement is to print some characters on to the display during boot-up (planning to make part of u-boot). Is it possible? First of all, printing on to LCD display is possible?
Regards,
Srikanth Vemula.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Srikanth
one can use sect.6.5.1 Framebuffer Tests attached Linux Manual and make fonts
in buffer, then send them to lcd.
mxc_fb_test\test - imx-test - i.MX Driver Test Application Software
For lvds one can look at Chapter 41 LVDS Display Bridge (LDB)
i.MX 6DualPlus/6QuadPlus Applications Processor Reference Manual
As it states: "The LVDS Display Bridge (LDB) connects the IPU (Image Processing Unit) to an
External LVDS Display Interface." IPU is described in Chapter 37, timings for both modules
can be found in i.MX 6DualPlus/6QuadPlus Applications Processor for Consumer Products Data Sheet
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------