Prevent current flowing back that MX8M processor and peripherals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Prevent current flowing back that MX8M processor and peripherals

2,270件の閲覧回数
bada
Contributor I

I have checked the I.MX8 reference design and have a question. 

Som board and carried board share a common power supply 1v8 and 3v3 through connectors.

Is it to prevent current backflow?

Can i design a i.mx8 som board +5v only supply? i.mx8 processor and peripherals IO use different 3.3v and 1.8v power supply.Not the same power rail.

0 件の賞賛
返信
4 返答(返信)

2,237件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Could you please share the schematic section that you are referring for?

It is ok if you need to supply your board with +5v only, if you need different voltage levels for each IO interface just use PMIC/discrete regulators to supply it.

Best regards.

0 件の賞賛
返信

2,217件の閲覧回数
bada
Contributor I
1.documnet number sch-46441,i.mx8m nano reference board.2.documnet number sch-29420,i.mx8qm cpu card.
Processor and peripherals IO use the same voltage
levels only not same power rail.For example,peripherals
power up first ,but Processor io unpower the moment.
Do current back flow to Processor io power?
0 件の賞賛
返信

2,201件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

No, there is no issue with that connection. Just keep power levels in operating range, follow the power-up sequence and you will be ok.

Best regards.

0 件の賞賛
返信

2,186件の閲覧回数
bada
Contributor I
It's ok.Thanks.
0 件の賞賛
返信