Common procedure for NAND programming i.MX27 is to use the ATK and application
note AN3985 "Customizing the Freescale Advanced Toolkit for i.MX Based Platforms"
(rev.0, 2/2010); in particular section 4 (Supporting a New NAND Flash Device).
http://www.freescale.com/files/dsp/doc/app_note/AN3985.pdf
"IMX_ATK_SOURCE_CODE"
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX27PDK&fpsp=1&tab=Design_Tools_Tab
For i.MX21 it is required to apply to similar ADS toolkit.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX21&fpsp=1&tab=Design_Tools_Tab
The idea is as following :
In engineering stage, we can use the ATK / ADS tool to download the image to the board so, that the board
can run. After that NAND may be demounted and read as is in binary from. For mass product, we need program
the NAND flash with an (external) programmer before mount them onto PCB. In order to work with most vendors
NAND programmers, bad block are skipped; and the programmer needn’t care the ECC method, just program the
data to NAND Flash.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------