Powering imx233 only by internal linear regulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Powering imx233 only by internal linear regulator

Jump to solution
1,446 Views
francescochino
Contributor I

Hi,

I need some example of imx-bootlet file to boot the imx233 using only the internal linear power supply. Is this code available? Could I send my code that needs to checked?

Thank you in advance for your support.

Regards

Francesco

Labels (1)
0 Kudos
Reply
1 Solution
1,305 Views
igorpadykov
NXP Employee
NXP Employee

HI Francesco

one can check 5V only mode, it is well tested on i.MX28 EVK

Updates and Patches (9)

Linux patch for i.MX28 SDK 2010.12 to add the most robust support

possible for a VDD5V or DCDC_BATT only configuration.

i.MX28 Evaluation Kit|Freescale

processor works from LDOs until hw_power_Enable4p2DcdcInput()

in hw_power.c imx-bootlets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,305 Views
francescochino
Contributor I

Hi Igor,

we have halfed the processor speed and now the board boots correctly.

Thank you for your support

My Best Regards

Francesco

0 Kudos
Reply
1,306 Views
igorpadykov
NXP Employee
NXP Employee

HI Francesco

one can check 5V only mode, it is well tested on i.MX28 EVK

Updates and Patches (9)

Linux patch for i.MX28 SDK 2010.12 to add the most robust support

possible for a VDD5V or DCDC_BATT only configuration.

i.MX28 Evaluation Kit|Freescale

processor works from LDOs until hw_power_Enable4p2DcdcInput()

in hw_power.c imx-bootlets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply