Power off sequence.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power off sequence.

Jump to solution
2,038 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.

The iMX6 is not specified of  power off sequence.

Phenomenon caused by the discharge of the capacitor speed and capacitance connected to the power supply.

For example, NVCC_EIM0 ~ 2 is at 3.3v, even if VDDARM_IN is like that 0.5v, Will it not be a problem?

If POR_B is negated, Would never like that, iMX6 to malfunction or failure?

Labels (1)
0 Kudos
Reply
1 Solution
1,859 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

no problem, as according to sect.4.2.2 Power-Down Sequence

i.MX6DQ Datasheet (rev.4, 7/2015)

No special restrictions for i.MX 6Dual/6Quad SoC.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

> If POR_B is negated, Would never like that, iMX6 to malfunction or failure?

no problem.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,860 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

no problem, as according to sect.4.2.2 Power-Down Sequence

i.MX6DQ Datasheet (rev.4, 7/2015)

No special restrictions for i.MX 6Dual/6Quad SoC.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

> If POR_B is negated, Would never like that, iMX6 to malfunction or failure?

no problem.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply