Power consumption estimation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power consumption estimation

4,215件の閲覧回数
niuweiqiang
Contributor I


Dear i.mx6 developer:

I am going to use i.mx6S processor.

But, I find a question during power consumption with the help of "iMX6X_Power_Tree_5Vin_separate" tool.

It is found that the parameter in line 17 impact the total power consumption greatly.

I can't confirm which value is suitable.

Can you give the advice or guide me confirm the actual value?

Thank you very much

Best regards.

0 件の賞賛
返信
4 返答(返信)

3,855件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share with us the file that you are refering ?.   You can check the application note

http://cache.freescale.com/files/32bit/doc/app_note/AN4715.pdf

This would provide Power Consumption Measurement numbers.

3,854件の閲覧回数
niuweiqiang
Contributor I

Hi Jamebone:

Thank you very much for your support.

I have checked the application Notes.

I find that the default resistor value is 120 ohm.

Please review below document in Line 17.

When the terminal resistor value is changed. The total power consumption

will be impacted.

Thank you very much

Best regards.

WeiQiang Niu

ABB Engineering (Shanghai)Ltd

No.5,lane 369,Chuangye Road,

Kangqiao Town,Pudong District,201319

Shanghai P.R.China

Phone: +86(21)6129 8121

Telefax: +86(21)6105 6905

Mobile: +86 1366 183 9086

email: [email protected]

0 件の賞賛
返信

3,853件の閲覧回数
YixingKong
Senior Contributor IV

Weiqiang

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

3,853件の閲覧回数
YixingKong
Senior Contributor IV

Weiqiang

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel

free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信