Power consumption (AN4270)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power consumption (AN4270)

1,177件の閲覧回数
MarkoPanger
Contributor III

Dear all,

I'm trying to evaluate the power consumption of a system around i.mx53. I've found an application note from Freescale which is based on some use cases:

http://cache.freescale.com/files/32bit/doc/app_note/AN4270.pdf

I'm particularly interested in the "Stop mode". According to the numbers given in the application note in this mode the DDR3 is operational and consumes 32mW out of a total of 36.5 mW.

Looking at the kernel sources this mode should put DDR3 in self-refresh mode and suspend itself into the internal RAM. In such a case I would expect a much lower power consumption for DDR3.

However those number are given for the Ubuntu image. Are they applicable also to the LTIB build ?

Thank, Marko

ラベル(1)
0 件の賞賛
返信
0 返答(返信)